Unable to init QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,873件の閲覧回数
salman83
Contributor I

Hi,

I am trying to initialize QSPI module on MCF52259. But reading and writing MCF_QSPI_QMR register causes an access error.

 

MCF_QSPI_QMR = (vuint16)(MCF_QSPI_QMR_MSTR | MCF_QSPI_QMR_BITS(12) | MCF_QSPI_QMR_BAUD(2))

 

I looked into the exception frame. It gives me "Error on operand read" when reading the register and "Error on operand write" while writing the register.

 

I do not know what causes the problem.

 

I even initialized the Port QS but still no luck.

 

Here is exception stack frame for both read and write

 

Read: - 0x4C082704

Write: - 0x48082708

 

Also, the error is not just related to one register. It causes problem with all QSPI registers.

 

Any help will be highly appreciated.

 

Regards.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,580件の閲覧回数
TomE
Specialist II

14.7.3.2 Peripheral Access Control Registers (PACR0–PACR10)

What's PACR4 set to?

Is your code executing in User Mode or Supervisor Mode?

> Read: - 0x4C082704     Format 4, FS 1100 (0xC), Vector 8, SR=2704

> Write: - 0x48082708      Format 4, FS 1000 (0x8), Vector 8, SR=2708

"Privilege violation" on Read and Write, just as you say.

The Status Register has the "Supervisor" bit set (0x2000), so you're not in User Mode.

IPSBAR has to be correct or you couldn't get to any peripherals.

Check that that "MCF_QSPI_QMR" definition is correct for your CPU. You may have the wrong header file in there somehow. Especially check the assembly code that is being generated.

Tom


元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,580件の閲覧回数
Monica
Senior Contributor III

Hello Salman!

Was that information helpful?

Please keep us posted, we'd like to know :smileywink:

Best regards,

Monica

0 件の賞賛
返信
2,580件の閲覧回数
salman83
Contributor I

I was missing PACR4.

0 件の賞賛
返信
2,580件の閲覧回数
TomE
Specialist II

> I was missing PACR4.

According to the manual, that register defaults out of reset to zero, which should allow Supervisor read-write. To block access, the bottom nybble must have been set to 0x07.

What software were you running that did that before your QSPI initialisation code?

Tom


0 件の賞賛
返信
2,580件の閲覧回数
TomE
Specialist II

14.7.3.2 Peripheral Access Control Registers (PACR0–PACR10)

What's PACR4 set to?

Is your code executing in User Mode or Supervisor Mode?

> Read: - 0x4C082704     Format 4, FS 1100 (0xC), Vector 8, SR=2704

> Write: - 0x48082708      Format 4, FS 1000 (0x8), Vector 8, SR=2708

"Privilege violation" on Read and Write, just as you say.

The Status Register has the "Supervisor" bit set (0x2000), so you're not in User Mode.

IPSBAR has to be correct or you couldn't get to any peripherals.

Check that that "MCF_QSPI_QMR" definition is correct for your CPU. You may have the wrong header file in there somehow. Especially check the assembly code that is being generated.

Tom


0 件の賞賛
返信