USB bootloader for MCF5225x or MCF52223

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB bootloader for MCF5225x or MCF52223

3,931 Views
Harjit
Contributor II
Hi.
 
A couple of days ago, I was surfing the freescale site and thought I had found source for the MCF5225x EVM or DEMOKIT or sample that had a USB boot loader that used the mass storage device model ala MCF51JM128.
 
I cannot for the life of me find it again.
 
Help!
Thanks,
Harjit
Labels (1)
0 Kudos
Reply
4 Replies

2,266 Views
RichTestardi
Senior Contributor II
Hi Harjit,
 
Is what you are looking for on the 5225x DVD-ROM at:
 
  D:\fscommand\MCF5225x_USB_BOOTLOADER.zip
 
This appears to be the subject of this lab tutorial:
 
 
For what it is worth, I run identical USB drivers on the 5225x, 52223, and 51JM128.
 
-- Rich
 
 
0 Kudos
Reply

2,266 Views
Harjit
Contributor II
Hi Rich.
 
Yes, that is the app. note for which I am looking for the sources for.
 
I cannot believe I can't find them any longer.
 
Are you using the sources from the demo kit disk or are you using the sources you've had from when you started on the 522xx or?
0 Kudos
Reply

2,266 Views
RichTestardi
Senior Contributor II
The source is on the MCF5225X Family Getting Started DVD that came with my M52259DEMOKIT at the path I indicated.
 
Do you have that DVD?
 
-- Rich
 
0 Kudos
Reply

2,266 Views
Harjit
Contributor II
 
Rich, it appears to be the same as what is on the DVD.
 
Thanks.
Harjit
0 Kudos
Reply