USB bootloader example. MCF52259DEMOMCU.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB bootloader example. MCF52259DEMOMCU.

1,868件の閲覧回数
Zaas
Contributor I
Is the USB bootloader example 'MCF5225x_Bootloader_with_Application' designed to load application code only once?.
ラベル(1)
0 件の賞賛
返信
1 返信

1,111件の閲覧回数
Zaas
Contributor I
Please, let me explain. I modified this bootloader 'MCF5225x_Bootloader_with_Application' slightly to work with serial interface using interrupts (Rx) instead of USB. Of course, I modified my applications as it is saying in 'M52259LAB.pdf' document to make it bootlader compatible.
 
I just try to do this sequence of uploads: My_SerialBootloader-->App1_BootCompatible-->App2_BootCompatible -->...

    I have problems when I tried to upload the code from App1_BootCompatible to App2_BootCompatible seems that when try to access to the variables related to the bootcode the programs hang up. I don't know what I'm missing or doing wrong? Could any one give me a little help or an idea about it?     

thanks in advance.
0 件の賞賛
返信