USB MSD Boot Loader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB MSD Boot Loader

1,355件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

 

A USB Mass Storage Device based boot loader has been added to the uTasker M522XX project. It can be seen in operation here: http://www.youtube.com/watch?v=H4TYM9jY2-g

 

The video shows the Kinetis K60 being used but the M522XX operation is identical [the hardware abstraction layer used allows Coldfire and Kinetis projects to be compatible] - details of the latest package for the M522XX are here: http://www.utasker.com/forum/index.php?topic=1310.0

 

Regards

 

Mark

ラベル(1)
0 件の賞賛
返信
1 返信

1,103件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

 

The USB-MSD boot loader has been extended to include password based software protection - this can be seen in operation in the following video: http://www.youtube.com/watch?v=e4oFBn_M5wo

 

Regards

 

Mark

 

P.S. The video shows the operation on a different chip but the code is also operational on the Coldfire :smileywink:

0 件の賞賛
返信