USB-ML-CFE Rev. D not working with CW 7.2  in debug mode with MCF52235

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB-ML-CFE Rev. D not working with CW 7.2  in debug mode with MCF52235

跳至解决方案
2,447 次查看
lupogrigio
Contributor III

Dear freescalers,

 

I reported here a problem found working with the Rev. D of the USB Coldfire Multilik debugger. In fact 

until yesterday I was working with success with the Rev. C of the debugger. Now, I have bought a new

MCF52235EVB board to do a new work, and that board arrived equipped with the Rev. D of the programmer.

 

Well, with this programmer I can't debug in RAM my applications. When I try to do this an error occurs (' loose of communication'). When I use my old programmer (Rev. C) this error does't occur, and I can debug with success 

my applications.

 

The erase and flash procedure work fine.

 

Some of you have a solution for this?

 

Thanks in advance for your attention.

标签 (1)
0 项奖励
回复
1 解答
1,578 次查看
lupogrigio
Contributor III

I' ve solved the problem.

 

The reason why both  USB-ML-CFE Rev. D and USB Multilink Universal don't work on CW 7.2 is the need to replace a .DLL file on the CW Program Folder.

 

Here the details:

 

To make the BDM works correctly is necessary to replace the file "unit_cfz.dll" in the folder: 
 
C:\Programmi\Freescale\CodeWarrior for ColdFire V7.2\bin\Plugins\Support\ColdFire\pemicro
 
with the newer version of the file attached to the post, that you can also find in the MQX Folder:
 
C:\Programmi\Freescale\Freescale MQX 3.8\tools\flash_programmer\CFFlashprog
 
I have attached to this mail the version of the file that I have received from the PE Micro Support Team.
 
Best Regards
 
L.
 
 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,579 次查看
lupogrigio
Contributor III

I' ve solved the problem.

 

The reason why both  USB-ML-CFE Rev. D and USB Multilink Universal don't work on CW 7.2 is the need to replace a .DLL file on the CW Program Folder.

 

Here the details:

 

To make the BDM works correctly is necessary to replace the file "unit_cfz.dll" in the folder: 
 
C:\Programmi\Freescale\CodeWarrior for ColdFire V7.2\bin\Plugins\Support\ColdFire\pemicro
 
with the newer version of the file attached to the post, that you can also find in the MQX Folder:
 
C:\Programmi\Freescale\Freescale MQX 3.8\tools\flash_programmer\CFFlashprog
 
I have attached to this mail the version of the file that I have received from the PE Micro Support Team.
 
Best Regards
 
L.
 
 

 

0 项奖励
回复
1,578 次查看
kenneth
Contributor I

Where is the file?

0 项奖励
回复