USB Bootloader for MCF51JM128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Bootloader for MCF51JM128

1,490 次查看
francescofalcin
Contributor I

Hello,
Long ago I developed an application with the ColdFire MCF51JM128 and the USB Bootloader (AN3748) on Code Warrior 6.1.
Now to update my application I used Code Warrior 10.4 always with the same bootloader.
The problem is that if I upgrade by connecting the PC usb to a card with the old firmware, upgrade is ok, but the ColdFire starts and goes reset, and so on.
If instead I program the MCU with the new FW through the Cyclone Pro and then I try to upgrade via PC, the MCU will run correctly.

You can help me ?

Thank you

0 项奖励
回复
1 回复

1,337 次查看
miduo
NXP Employee
NXP Employee

Hi,

Sorry I am not quite understand what your meaning. What OS are you using for CW and have you update the GUI for the bootloader?

0 项奖励
回复