TCP/IP solution for MCF523x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TCP/IP solution for MCF523x

3,189件の閲覧回数
Arev
Contributor III

Hello,

 

I'm using a Freescale MCF5234/5235 and need to support the following Ethernet protocols

 

TCP/UDP/IP

DHCP (RFC2131)

DNS (RFC1034,RFC1035)

IGMP v2 (RFC2236)

DiffServ (RFC2474)

NTP v3 (RFC1305)

VLAN (IEEE802.1Q)


Does anyone know a RTOS and IP Stack that support these protocols for my platform.

 

VLAN, NTP and DiffServ are not supported by a lot of embedded systems.


Thanks for help

 

Bye,

 

<< Freescale MCF5234/35 with CodeWarrior 6.4 >>

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,934件の閲覧回数
ChrisJohns
Contributor I

Hi,

 

I have not run these specific protocols but many others not normally found in embedded real time system such as IMAP using RTEMS. The way I did this was to embed Python. It comes with all sorts of excellent and well written protocols including (from a quick Google) WSDL and SOAP. Things like NTP are directly supported by RTEMS.

 

I found the performance compared to the traffic flow acceptable and I still had RTEMS running all the real time parts of my application written in C++. The ability to just include a protocol and play was fastastic. We ended up writing parts of the application that handled the data in Python and just loaded the compiled Python code on the target file system.

 

RTEMS is http://www.rtems.org/

 

Regards

Chris

0 件の賞賛
返信

1,934件の閲覧回数
Arev
Contributor III

Hello,

 

I need also to support

 

WSDL and SOAP


Bye

0 件の賞賛
返信

1,934件の閲覧回数
sirlenzelot
Contributor II

Hi Arev,

have a look at Nucleus by Mentor Graphics. I'm not sure whether they support all of your wishes, but I know that there exist OSS SOAP Server, which you can implement.

 

vy73

Dirk

0 件の賞賛
返信