TCP/IP Dual-Stack (IPv4/IPv6) for M522xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TCP/IP Dual-Stack (IPv4/IPv6) for M522xx

1,689 次查看
mjbcswitzerland
Specialist V

Hi All

The latest uTasker release for the M522xx contains advanced IPv6 support for TCP based services (web server, TELNET, FTP etc.). Details and download of the release V1.4.11 for Coldfire V2 are at http://www.utasker.com/forum/index.php?topic=1310.0

The IPv6 user's guide is at http://www.utasker.com/docs/uTasker/uTaskerIPV6.PDF explaining the operation and detailing methods of utilising IPv6 services on Coldfire V2 devices (the dual-stack operation adds only about 6k additional Flash footprint on the Coldfire) in a local network or in the Internet. The dual-stack supports 6in4 tunnelling to allow multiple IPv6 globally addressed devices to be located behind 'old' IPv4 gateways - theoretically this allows up to 2^64 IPv6 capable devices to be positionen behind a single IPv4 addressed gateway !! (eg. huge amounts of IPv6 global web servers on port 80, each globally addressable from the IPv6 Internet, even when providers can't offer IPv6 services directly). This opens up many new potentials (even before IPv4 addresses finally run out

The same support will be released for the Kinetis project too during the next days.

Regards

Mark


P.S. A new IPv6 discussion board has been started for interested developers: http://www.utasker.com/forum/index.php?board=11.0

标签 (1)
0 项奖励
回复
1 回复

1,240 次查看
Luis_Garabo
NXP TechSupport
NXP TechSupport

Thanks for the information Mark!!

Best Regards,

Garabo

0 项奖励
回复