Switching mini-flexbus modes during runtime on M5225x, M52259

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Switching mini-flexbus modes during runtime on M5225x, M52259

ソリューションへジャンプ
5,183件の閲覧回数
juanee
Contributor III

Hello everyone,

 

I am new to the M52259 Coldfire and I have read the AN3854 Mini-FlexBus.pdf (Rev. 0, 04/2009) application note concerning this topic.

 

My question... am I able to switch mini-flexbus modes (non-multiplexed to multiplexed and back again) at any time during runtime?

 

The reason:  I wanted to control an asyncronous RAM (that has a 16 bit data bus) and a Flash NAND (that has an 8 bit data bus), but I wanted to have 16 bit data access to the RAM).

 

thanks,

juanee

ラベル(1)
0 件の賞賛
返信
1 解決策
3,340件の閲覧回数
juanee
Contributor III

"Am I able to switch back and forth between the mini-flexbus mode and general purpose IO (PTE, PTF PTG, etc) during runtime?"

 

To answer my own question, the answer is YES.  I have an external memory on the mini-flexbus that also needs the PTE, PTF ports as GPIO (to interface to another device).

 

Juan

 

Codewarrior 10 Special Edition

Windows XP Pro

MQX 3.6.2

PEMicro USB ColdFire Multilink.

Custom Target based on Coldfire MCF52259.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,340件の閲覧回数
usingbothmuxand
Contributor II

Hi everybody,

           Anybody plz reply me.

Is FB_ALE/FB_CS1_BAR may work as FB_ALE in mux mode and FB_CS1_BAR in non-mux mode for different chip selects at run time? Bcs i need minimum two chip selects in my system...

Is My design right?

 

Thanx...

0 件の賞賛
返信
3,340件の閲覧回数
scifi
Senior Contributor I

Hi Juanee,

 

Have a look at register definitions for CSCR0 and CSCR1. You will find that each chip select has independently configurable multiplexed mode and bus width.

 

Regards,

- mike

 

0 件の賞賛
返信
3,340件の閲覧回数
juanee
Contributor III

Hello Mike,

 

I read what you suggested and I understand better now how it works.  Thanks.

 

But, another question though...

 

Am I able to switch back and forth between the mini-flexbus mode and general purpose IO (PTE, PTF PTG, etc) during runtime?

 

Thanks,

juanee

 

0 件の賞賛
返信
3,341件の閲覧回数
juanee
Contributor III

"Am I able to switch back and forth between the mini-flexbus mode and general purpose IO (PTE, PTF PTG, etc) during runtime?"

 

To answer my own question, the answer is YES.  I have an external memory on the mini-flexbus that also needs the PTE, PTF ports as GPIO (to interface to another device).

 

Juan

 

Codewarrior 10 Special Edition

Windows XP Pro

MQX 3.6.2

PEMicro USB ColdFire Multilink.

Custom Target based on Coldfire MCF52259.

0 件の賞賛
返信
3,340件の閲覧回数
scifi
Senior Contributor I

juanee wrote:
Am I able to switch back and forth between the mini-flexbus mode and general purpose IO (PTE, PTF PTG, etc) during runtime?

I think you should be able to do this. I haven't tried this myself, though...

 

0 件の賞賛
返信
3,340件の閲覧回数
usingbothmuxand
Contributor II

I am facing same problem with this device.

my RAM is accessed as x8 bit and EoPDH device as x16 bit peripheral.

Is it possible to use FB_ALE/FB_CS1_BAR as FB_ALE in multiplex mode and as FB_CS1_BAR in non-multiplex while external devides are selecting by CS0 and CS1 signal?

 

See my block diagram...for that I have attached it.

FB_ALE/FB_CS1_BAR is routed to RAM and x16 latch by FB_CS0_BAR.

conditions is:::

 

if(FB_CS0_BAR==0)

            FB_ALE <= FB_ALE/FB_CS1_BAR       // to x16 latch

else

            FB_CS1_BAR <= FB_ALE/FB_CS1_BAR     // to RAM

 

Thanx...

0 件の賞賛
返信