Subject: How can we prevent a receive FIFO overrun on an MCF5372  FEC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Subject: How can we prevent a receive FIFO overrun on an MCF5372  FEC

1,257 Views
sambuharikrishn
Contributor I

We have an MCF5372 chip.Randomly we are getting overrun error in receive side.Receive data rate is  every one milli second 550 bytes of data is received.
The OV bit is set in the receive buffer and the count of "receive fifo overruns" is incremented.

As per the reference manual OV bit is set only for the below reason

19.5.15.2.1 Overrun Error
If the receive block has data to put into the receive FIFO and the receive FIFO is full, FEC sets RxBD[OV].
All subsequent data in the frame is discarded and subsequent frames may also be discarded until the
receive FIFO is serviced by the DMA and space is made available. At this point the receive frame/status
word is written into the FIFO with the OV bit set. The driver must discard this frame.

But the behaviour in my controller is different we have free descriptors but still overrun is set.
We have 16 descriptors each one with the size of 256*7 bytes.Incoming data maximum size observed is 550 bytes
When the overrun is observed i have displayed all the descriptors.
Below is the attached capture when overrun is occured

I/O: index 0
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 1
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status802
I/O: nx_mcf5372_record.pRxDescTableStart[i].length22a
I/O: index 2
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status800
I/O: nx_mcf5372_record.pRxDescTableStart[i].length71
I/O: index 3
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status800
I/O: nx_mcf5372_record.pRxDescTableStart[i].length71
I/O: index 4
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 5
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 6
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 7
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 8
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 9
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 10
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 11
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 12
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 13
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 14
I/O:  nx_mcf5372_record.pRxDescTableStart[i].status8000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0
I/O: index 15
I/O:  nx_mcf5372_record.pRxDescTableStart[i].statusa000
I/O: nx_mcf5372_record.pRxDescTableStart[i].length0

Please let me know why overrun is occurred still there are free descriptors.

Labels (1)
0 Kudos
Reply
1 Reply

1,064 Views
TomE
Specialist II

Have you searched this forum for "FEC Overrun"? There are quite a few previous instances that might be of use.

How have you got the Crossbar Switch set up? The FEC DMA must be higher priority than the CPU. Do you have USB?

Here's one with a lot of details where the symptom was a failed TRANSMIT with Underrun. That was due to the Reference Manual not having a sentence that was in nearly all other device manuals, which is to be sure to initialise R_FSTART.

https://community.nxp.com/message/407754?commentID=407754#comment-407754 

Here's a good one where the poster "found the problem", but his explanation didn't make sense. Lots of things to read and try in these, anyway:

How can we prevent a receive fifo overrun on an MCF5235 FEC 

There are a lot of people successfully using the FEC on these parts without any problems. If you have a problem it is most likely to be a software bug where you're not "doing the right thing by the chip". But finding out what that is is usually more than reading the manual.

Tom

0 Kudos
Reply