Strange problem with LTIB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Strange problem with LTIB

4,445 次查看
JimDon
Senior Contributor III
I am using the version that comes with the M2277EVM BSP.

It keeps forgetting the path to the complier. It seems to save it in the config file, but when I go back to config mode again, it is blank, so I would say it fails to read it back.

It does remember the compiler prefix ok.
I am using the compiler that comes with CW for Linux, so the path is pretty long. Is there a length limit?

标签 (1)
0 项奖励
回复
6 回复数

2,729 次查看
mwaddel
Contributor I
Is there an entry in the config/platform/m5227xevb/defconfig.dev
file after you save the configuration?  When I select the custom
toolchain option and save this is what I see in the that file:

...
#
# Toolchain selection.
#
# CONFIG_TOOLCHAIN_68KNOMMU_UCLIBC1 is not set
CONFIG_TOOLCHAIN_68KNOMMU_CUSTOM=y
CONFIG_CUSTOM_TOOLCHAIN=y
CONFIG_TOOLCHAIN_PATH="/opt/freescale/usr/local/gcc-4.2.20-uclibc-0.9.20/m68k-uclinux/"
CONFIG_CUSTOM_TOOLCHAIN_PREFIX="m68k-uclinux-"
CONFIG_TOOLCHAIN_PREFIX="m68k-uclinux-"
CONFIG_TOOLCHAIN_CFLAGS=""
...

If the CONFIG_TOOLCHAIN_PATH isn't correct then there could be a problem
in LTIB.

--Matt
0 项奖励
回复

2,729 次查看
JimDon
Senior Contributor III
Yes, it goes into the config file and the build works.
And it does seem to be in the config file if you look.
I just have to put it back each time I go into config, as it is blank.


0 项奖励
回复

2,729 次查看
JimDon
Senior Contributor III
Code:
#
# Choose your toolchain
#
# CONFIG_TOOLCHAIN1 is not set
CONFIG_TOOLCHAIN_CUSTOM=y
CONFIG_TOOLCHAIN_PATH="/opt/freescale/usr/local/gcc-4.2.47-uclibc-0.9.47/m68k-uclinux"
CONFIG_CUSTOM_TOOLCHAIN_PREFIX="m68k-uclinux-"
CONFIG_TOOLCHAIN_PREFIX="m68k-uclinux-"
CONFIG_TOOLCHAIN_CFLAGS="-mcpu=5329 -DCONFIG_COLDFIRE"

And after running --config

# Choose your toolchain
#
# CONFIG_TOOLCHAIN1 is not set
CONFIG_TOOLCHAIN_CUSTOM=y
CONFIG_TOOLCHAIN_PATH=""
CONFIG_CUSTOM_TOOLCHAIN_PREFIX="m68k-uclinux-"
CONFIG_TOOLCHAIN_PREFIX="m68k-uclinux-"
CONFIG_TOOLCHAIN_CFLAGS="-mcpu=5329 -DCONFIG_COLDFIRE"


 BTW Should I clear the CFLAGS like you did?
0 项奖励
回复

2,729 次查看
JimDon
Senior Contributor III
Well, here is part of the problem:
If I enter the path as:
/opt/freescale/usr/local/gcc-4.2.47-uclibc-0.9.47/m68k-uclinux/
It remembers it.
However then the build fails:

Code:
Found m68k-uclinux-gcc through your PATH at:/opt/freescale/usr/local/gcc-4.2.47-uclibc-0.9.47/m68k-uclinux/bin/m68k-uclinux-gccExpected to find it at:/opt/freescale/usr/local/gcc-4.2.47-uclibc-0.9.47/m68k-uclinux//bin/m68k-uclinux-gcc

 

If I leave off the '/' at the end the build works...but it forgets the path.
On the other hand, if I use:
/home/myusername/CodeSourcery/Lite
(where I installed the download from CodeSourcery)
It both remembers it and works, so something is up with LTIB and the path name.






Message Edited by JimDon on 2008-06-24 10:32 PM

Message Edited by JimDon on 2008-06-24 10:39 PM
0 项奖励
回复

2,729 次查看
mwaddel
Contributor I
Hi Jim,

With these instructions I was able to duplicate the failure you are seeing.  I
also noticed, the TOOLCHAIN_CFLAGS setting disappears also.

I think I've found the problem and I've sent a solution to the LTIB developer. 
I want to make sure the fix doesn't break something else.  I'll let you know
as soon as it's ready.

In case you're interested, there is a specific LTIB developers mailing list at:
http://savannah.nongnu.org/projects/ltib/

Regards,
Matt
0 项奖励
回复

2,729 次查看
JimDon
Senior Contributor III
Wow! Thank you!!!!

I do subscribe to that list, but I thought since it was a Freescale distro, somebody here might be more interested in looking at it.

Now I am a little paranoid that other settings might have been changed from the default. I am new to this, and it is a bit overwhelming at first, so I have been just trying to duplicate the original images with default settings.

Please advise when and where I can get the update for this.
0 项奖励
回复