SetStopMode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SetStopMode

1,517件の閲覧回数
néfiarmelim
Contributor II

Hello, I am using MC51EM in a project and now I need to apply the SetStopMode function , I use the Processor Expert 6.3. However, the option help doesn't have the example.

 

I need the minimum consumption in my application.

 

I read the chapter 6 of reference manual, but how I apply it?

 

I get to use the function but the MCF51EM doesn't back to work, How can I do it?

 

Regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,447件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

To activation SetStopMode function it is necessary to enable STOP instruction. The "Clock settings - Low Power Mode settings - STOP instruction enabled" property should be set to "yes" value in CPU Inspector window - Properties page.

 

0 件の賞賛
返信