Hi,
I am trying to design a communication protocol between the 5282 and a PC.
The 5282 sends characters from 0 to 0xFF and the PC is supposed to read them.
The problem I am having is reading the zeros! All other values (from 1 to 0xFF) work fine.
The code of the PC program is (in a while loop with timeouts):
Code:
unsigned char c;ReadFile(handle, &c, 1, &n_bytes_read, NULL);// read 1 character at a time
When the firmware sends a 0 integer, the ReadFile() function returns with n_bytes_read = 0.
So there is no way finding out if ReadFile() didn't read any value OR it read a 0 integer (which is the NULL character in ASCII).
I know that this is not a 5282 problem but rather a kernel32 but I thought someone might have solved this
issue.
Thanks,
S.