SDRAM connections MCF5208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM connections MCF5208

4,575 Views
fevernova
Contributor I
Hi at all,
 
I will develop a board with the mcf5208. :smileysurprised:
Now I will know how to connect one or two (assembly option) respectively sdrams (K4S281632) to the cpu.
These signals are clear to me: -1st sdram D16-D31 to dq0-dq15
                                                  -dqm3 to udqm
                                                  -dqm2 to ldqm
 
                                                  -2nd sdram D0-D15 to dq0-dq15
                                                  -dqm1 to udqm
                                                  -dqm0 to ldqm
 
And what's about the address lines and chip selects? :smileymad:
Same address lines in 16bit and 32bit?
One chip select for both modes (16/32bit) or two?
 
 
thx
 
fevernova
Labels (1)
0 Kudos
Reply
5 Replies

2,569 Views
UK_CF_FAE
NXP Employee
NXP Employee
Hello FeverNova,
 
I diodn't look up those memory chips. I guess that they are by-16 architecture. Since the ColdFire has byte addressability, then you need to connect the A0 from the mcu to the A1 on the memory, etc. From your description of what you know already, you seem to want to make a 32-bit wide memory from the 2-off x16 parts, that's why you'd connect the D16 to dq0 on the first sdram. Then you say its a assembly option, which puzzled me.
 
2 references for you to look at:
1) Schematic for the MCF5208 eval board, published to the freescale site
2) FlexBus application note AN2982.
 
Good luck
 
Mark
0 Kudos
Reply

2,569 Views
fevernova
Contributor I
...let's start new. :smileysurprised:
I will use sdram by 16bit architecture (k4s281632I-ui75) and flash (s29gl032a90tfir4) by 16bit architecture.
 
So I'll take a full 32bit bus mode for 32bit sdram controller and 32bit for flexbus (dramsel=1).
As standard memory I will use one 16bit sdram and so I thought I have to connect the sdram to the upper data lines of the sdram controller:
sdram dq0=cpu d16
sdram dq1=cpu d17
...
sdram dq15=cpu d31
sdram ldqm=cpu sddqm2
sdram udqm=cpu sddqm3
sdram cs=cpu sdcs0
sdram a0=cpu a0
sdram a1=cpu a1
...
sdram a10=cpu sd_a10
...
sdram n.c./a12=cpu a12
sdram ba0=cpu a14
sdram ba1=cpu a15
 
And here isthe flash connection:
flash a0=cpu a1
flash a1=cpu a2
...
flash n.c./a21=cpu a22
flash cs=cpu cs0
flash dq0=cpu d16
flash dq1=cpu d17
...
flash dq15=cpu d31
 
refer to page 287 (flexbus, data byte alignment) in manual.
 
A an assembly option I will use a second sdram by 16bit to built a 32bit architecture by 2x16bit.
So I take the second sdram and connect it in this way:
sdram dq0=cpu d0
sdram dq1=cpu d1
...
sdram dq15=cpu d15
sdram ldqm=cpu sddqm0
sdram udqm=cpu sddqm1
sdram cs=cpu sdcs0
sdram a0=cpu a0
sdram a1=cpu a1
...
sdram a10=cpu sd_a10
...
sdram n.c./a12=cpu a12
sdram ba0=cpu a14
sdram ba1=cpu a15
 
Is it  the correct connection?
 
I hope it is understandable.
 
thx, fevernova
0 Kudos
Reply

2,569 Views
fevernova
Contributor I
Does anybody has an idea?
 
best regards...René
 
0 Kudos
Reply

2,569 Views
Maybar
Contributor I
Did you resolve the problem?
I have the same question:
Coldfire 5208 in 32 bit mode.
Flash and SDR RAM with 16 bit size.
Is correct to connect cpu(A1-A21) to Flash[A0-A20]?
Thanks,
Miguel.


0 Kudos
Reply

2,569 Views
fevernova
Contributor I
I think so. Refer to 17.3.1.1 Port Sizing in Manual.
 
Bye
 
0 Kudos
Reply