SDHC card MISO Remains Low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDHC card MISO Remains Low

ソリューションへジャンプ
1,733件の閲覧回数
Dave_W
Contributor I

Hi

 

I'm having an issue communicating with my SDHC card.  I should mention that I have communicated with this card before with the same code on a slightly older version of the circuit. 

 

The mcf51 is communicating with the card via SPI via potential dividers on CS, MOSI and SCK as the micro is running at 5V to fulfill several other requirements.  The MISO line is put through a hex inverter to buffer the signal up to 5V.

 

I have not connected any pullup resistors anywhere, but I assumed that it wasn't necessary given that first prototype I made worked without them with this same card.

 

Essentially I get no response from the card.  The MISO line remains Low all the time.  Can anyone suggest a potential reason for this?

 

Thanks in advance


Dave Wright

ラベル(1)
0 件の賞賛
返信
1 解決策
1,541件の閲覧回数
Dave_W
Contributor I

It was not quite as 2 dimensional as that, there were no changes in the electrical schematic only in the PCB layout so there should have been no hardware induced issues. 

 

I was hoping there was a common problem that caused a low MISO but I couldn't find anything on forums.

 

However I solved the issue, it came down to a poor contact that was hidden under the smd sd socket.  It wasn't immediately clear even with a microscope.

 

Thanks for the response.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,541件の閲覧回数
FridgeFreezer
Senior Contributor I

So it was working, then you changed the circuit and it doesn't work anymore. I think there's a clue there :smileywink:

 

What does the electrical specification say for each of the devices you're using?

0 件の賞賛
返信
1,542件の閲覧回数
Dave_W
Contributor I

It was not quite as 2 dimensional as that, there were no changes in the electrical schematic only in the PCB layout so there should have been no hardware induced issues. 

 

I was hoping there was a common problem that caused a low MISO but I couldn't find anything on forums.

 

However I solved the issue, it came down to a poor contact that was hidden under the smd sd socket.  It wasn't immediately clear even with a microscope.

 

Thanks for the response.

0 件の賞賛
返信