Search finds a very similar question with good answers from Freescale in 2010:
https://community.freescale.com/message/67779#67779
That's also a good answer from Hao Wang.
The MCF5475 and MCF5485 manuals are identical in the Supply Voltage Sequencing. The MCF54418 and MCF54452 manuals are the same. The MCF53017 is the most interesting as it has the "0.4V restriction" part printed in RED, like it is the first one to be edited this way (or it is VERY important :-).
These other manuals have recommendations that aren't in the one for your part. But they are also somewhat contradictory as they state both:
- Recommended that IVDD/PLL VDD should track EVDD/SD VDD up to 0.9V, then separate for completion of ramps.
- If EVDD/SD VDD are powered up with the IVDD at 0V, ...
So it recommends it tracks but it isn't required. Are there any advantages to the recommendation or disadvantages to not following it?
Maybe the latter condition forces all pins to high impedance, including some pins that otherwise wouldn't be in that state. So designs that power up that way might require external resistors (to establish a default state for external hardware) that wouldn't be necessary with the other power sequencing scheme.
I miss CPUs that had a single power supply (I'm also working with the i.MX53:-).
Tom