Question about FlexCAN message buffers behaviour

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about FlexCAN message buffers behaviour

1,935件の閲覧回数
neodelphi
Contributor I
Hi !

I am currently working on a Coldfire MCF5235, which includes the FlexCAN module. I've made the CAN bus working but there is something I don't understand very well. Indeed I configured three message buffers as input. There are no Id masks at all and all receive buffers have the same configuration. Now suppose a device sends me two CAN messages. The first message will be stored in MessageBuffer1, an exception will be generated... If my program locks the message buffer once exception is triggered, and don't release it, will the second CAN message be stored in the MessageBuffer2 ?

Thanks for answering !
Olivier Heriveaux
ラベル(1)
0 件の賞賛
返信
1 返信

1,153件の閲覧回数
krsihna1234
Contributor I
HI,
 
    Have you written drivers for mcf5235 ? If you can you send me the source ? Actually I want to write drivers for MCF5282 so I would like to understand the code.
 
Thanks
krishna
0 件の賞賛
返信