Programming through the TWR-MCF51CN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming through the TWR-MCF51CN

1,580 Views
AceMax
Contributor I

Hello,

 

I bought the TWR-MCF51CN. The User Manual says:

 

"6.2 Stand-Alone Debug Interface
The OSBDM circuit is designed so that it can program the on-board MCF51CN device, or be isolated
from the on-board circuitry and be used as a programmer for other ColdFire V1 devices. The steps
necessary to operate the OSBDM in this mode are listed here:
1. Remove 0 ohm resistor, SH1
2. Connect J8 (2x3 header) from TWR-MCF51CN to target debug connector"

 

So, as far as I understood, It's possible to program my prototype board through the Tower System. Am I right?

 

The question is that when I try to download the code to prototype board CodeWarrior don't find the hardware.

 

 

Does anyone succeed in program the uController throught the Tower System? Got any problem?

 

Best regards!

 

 

André Fernandes

Message Edited by AceMax on 2010-01-13 06:32 PM
Labels (1)
0 Kudos
Reply
1 Reply

1,197 Views
AceMax
Contributor I
Please. Does anybody known if there is any specific configuration or sequence to program the MCF51?
0 Kudos
Reply