Problems with interrupt handling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems with interrupt handling

1,576 次查看
Richmand
Contributor II

Hi. I've got the following problem and I hope anyone can help me.

 

I want to build up a small CAN network with MCF52235 and therefor I want to use an interrupt controlled message receive, so every successful received message is caught by the ISR.

 

For the first tests, I enabled the interrupt sources for the flexcan message buffers with interrupt level and priority, set all IMASK bits in flexcan module and put the interrupt handlers in the vector table. But when I start the transmission and the IFLAG bit for successful transmit is set, no interrupt occurs.

 

In the attached files are the exceptions.c with the vector_table, MCF52235_INTC.h with ISR prototypes and MCF52235.c with interruptcontroller initialization and the ISR functions.

 

I hope anyone can tell me where I did something wrong.

 

Best regards

 

exceptions.c

MCF52235_INTC.c

MCF52235_INTC.h

Message Edited by t.dowe on 2009-11-18 10:57 AM
标签 (1)
0 项奖励
回复
1 回复

991 次查看
mjbcswitzerland
Specialist V

Hi

 

    MCF_INTC0_IMRH = 0xFFFFFFFF;   /* Masks all interrupts in IMRH */
    MCF_INTC0_IMRL = 0xFFFFFFFE;   /* Masks all interrupts in IMRL */
    MCF_INTC1_IMRH = 0xFFFFFFFF;   /* Masks all interrupts in IMRH */

Check that you are allowing CAN interrupts by 'clearing' the appropriate bits in MCF_INTC1_IMRH.

 

These are

  #define CAN_TX_INTS_L     0x0000ff00                                   // Interrupt controller 1
  #define CAN_RX_INTS_L     0x00ff0000                                   // Interrupt controller 1
  #define CAN_ERR_INT_L     0x01000000                                   // Interrupt controller 1
  #define CAN_BOFF_INT_L    0x02000000                                   // Interrupt controller 1

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

0 项奖励
回复