Problems using Windows 10 and  AN3927 (USB Bootloader MSD) framework, SF734138

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems using Windows 10 and  AN3927 (USB Bootloader MSD) framework, SF734138

2,501 Views
dirkricker
Fresh Out Contributor

I am currently using the  AN3927 (USB Bootloader MSD) framework to update our product that uses a MCF51JM128.  I am having issues with updating the firmware with Windows 10.  It pops up as a drive on my host computer and I am able to copy to it, but after reboot it always fails with a SF734138 error.  Still works fine with Windows 7, but less and less of our customers have a machine running 7 or XP. 

Labels (1)
0 Kudos
Reply
2 Replies

2,318 Views
miduo
NXP Employee
NXP Employee

Hi,

Actually I am still not updated to WIN 10. So for your case, you may make reference below tread:

https://mcuoneclipse.com/2013/12/14/new-pe-opensda-firmware-v114/ 

P&E had update the OpenSDA driver for Win 8.1, not sure if work for Win 10, You can try.

2,318 Views
dirkricker
Fresh Out Contributor

Thanks Fang, I will give this a look

0 Kudos
Reply