Problem with the frame buffer of MCF5329

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with the frame buffer of MCF5329

1,872件の閲覧回数
Dome
Contributor II
Hi,

when I use the MCF5329 with a resolution of 800x480, I have the follow problem:
if the frame buffer is black (ex.: "cat /dev/zero > /dev/fb0") the throughput over ethernet is about zero, it's diffucult to ping the board. Instead if the frame buffer is colored or white better the throughput is ok, we arrived about to 10 Mbit/s.
Why there is this difference?

Thanks
Bye
Dome
ラベル(1)
0 件の賞賛
返信
1 返信

1,128件の閲覧回数
obidon
Contributor III
You might check your crossbar switch module priorities XBS_PRS1. I know with a 640 x 480 LCD running 18bpp it is necessary to boost the LCD controller priority to prevent steaks on the display. This slows everything else. For our current project we are using 8bpp with a lower priority on the LCD controller.
0 件の賞賛
返信