Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0

1,767件の閲覧回数
K8Lxqg
Contributor I

Hi!

 

I'm trying to transmit data between PC and M52223EVB via USB (J1 plug-in). I try to use cdc-demo in CMXUSB example program package. When I make the project I receive the following error:

 

Link Error: Undefined: "_start"

 

For some reason I couldn't install Windows DDK to my PC with XP SP3. Is that the reason of the error? Is there a possibility that I can use CDC Demo without DDK?

 

Thanks in advance,

 

Teoman

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,238件の閲覧回数
K8Lxqg
Contributor I
Wrong CW Version info sorry, I'm using CW 7.1.2
0 件の賞賛
返信

1,238件の閲覧回数
PaoloRenzo
Contributor V

Did you try the flash programmer utility for the mcf52223 MCU?

 

DDK utility is not needed to run CDC

 

Windows will ask for INF file provided with the ZIP as soon as USB device is recognized

 

Probably the DDK you're referring to is the Windows Studio project that needs DDK to recompile the HID source code, which at runtime is not needed at all.

 

Hope this helps

0 件の賞賛
返信