Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0

1,755 Views
K8Lxqg
Contributor I

Hi!

 

I'm trying to transmit data between PC and M52223EVB via USB (J1 plug-in). I try to use cdc-demo in CMXUSB example program package. When I make the project I receive the following error:

 

Link Error: Undefined: "_start"

 

For some reason I couldn't install Windows DDK to my PC with XP SP3. Is that the reason of the error? Is there a possibility that I can use CDC Demo without DDK?

 

Thanks in advance,

 

Teoman

Labels (1)
0 Kudos
Reply
2 Replies

1,226 Views
K8Lxqg
Contributor I
Wrong CW Version info sorry, I'm using CW 7.1.2
0 Kudos
Reply

1,226 Views
PaoloRenzo
Contributor V

Did you try the flash programmer utility for the mcf52223 MCU?

 

DDK utility is not needed to run CDC

 

Windows will ask for INF file provided with the ZIP as soon as USB device is recognized

 

Probably the DDK you're referring to is the Windows Studio project that needs DDK to recompile the HID source code, which at runtime is not needed at all.

 

Hope this helps

0 Kudos
Reply