Possible mistake in MCF52259 Coldfire Integrated Microcontroller Reference Manual MCF52259RM Rev.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Possible mistake in MCF52259 Coldfire Integrated Microcontroller Reference Manual MCF52259RM Rev.2

ソリューションへジャンプ
3,449件の閲覧回数
sven_kaemmer
Contributor III

Hello,

 

is it possible that in the MCF52259 Coldfire Integrated Microcontroller Reference Manual MCF52259RM Rev.2" is an mistake in chapter "30.5.2 ADC Sample Conversion"?

 

...Thus a complete 12-bit comversion takes 6 ADC clocks (1.2ms)...

 

I think this should be 0.0012ms. Is this ok?

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,021件の閲覧回数
J2MEJediMaster
Specialist I

I will pass this information to the documentation people. No sense in confusing developers.

 

Thank you for reporting this.

 

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,021件の閲覧回数
scifi
Senior Contributor I

Obviously, this is a typo. They meant microseconds, not milliseconds.

Hey, they are only humans. Of course mistakes are possible.

0 件の賞賛
返信
2,021件の閲覧回数
sven_kaemmer
Contributor III

Hi scifi, thanks for your answer. You are right. I also think so.

I posted this message for people they read this manual first and then this typo can be confusingly.

 

Have a nice day...

0 件の賞賛
返信
2,022件の閲覧回数
J2MEJediMaster
Specialist I

I will pass this information to the documentation people. No sense in confusing developers.

 

Thank you for reporting this.

 

---Tom

0 件の賞賛
返信
2,021件の閲覧回数
sven_kaemmer
Contributor III

Thank you Tom.

0 件の賞賛
返信