Hello-
On the PIC series of Microcontollers I can do the following:
#pragma udata myData=0x2000
unsigned char value;
/*
any other variables I wish to declare
*/
#pragma udata
This will place the variable 'value' at memory location 0x2000 in RAM with any other variables following consecutively after that until the subsequent pragma. I'd like to know how to do this same process on the MCF52233. I found a pragma that looked very similar to what I wanted, but it didn't use any numbers so I wasn't clear on how I could tell exactly where in memory that section would go. The pragma I found appeared to allow me to name a section of memory but that section could still be placed in an arbitrary memory location. How do I place data exactly where I want it?
You typically have 2 ways. The first way is C with no specific tricks:
#define UDATA_BASE ((unsigned char*) 0x2000)
#define value *(UDATA_DATA + 0)
If you have a few variables at this address place them in a structure.
The second way is to use the linker command file and that depends on your compiler. The manual should contain examples.
 
					
				
		
 
					
				
		
Dear eqqman,
The example given by Chris is correct. value is an lvalue.
Another alternative that is codewarrior specific is to use the '@' notation as shown in the examples below:
 
int example1@0x1000; // Codewarrior specific method
#define EXAMPLE2 (*(volatile unsigned int *) 0x1000)  // Standard C
int main(void)
{
   example1 = 0x12345678;
   EXAMPLE2 = 0x12345678;
  
}
 
Both assignments produce similar code. The second is more portable but since accesssing a specific location is almost certainly target specific I can't really see much argument about this being an advantage.
The advantage of the 1st is that example1 will appear as a variable in the debugger - EXAMPLE2 is invisible since while an lvalue it's not actually a named variable, just pointer magic.
bye
 
					
				
		
Ah-
So if I have
struct globals{
/* dat atype 1 */ value1;
/* datatype 2, etc. */ value2;
};
I can do
#define MEMORY (*(volatile globals *) 0x1000)
MEMORY.value1 = whatever
without any of the structure members being named in the debugger?
 
					
				
		
Dear Eqqman,
That looks about right but I would prefer the @notation.
A more complete example:
int example1@0x1000;
#define EXAMPLE2 (*(volatile unsigned int *) 0x1000)
typedef struct
{
   int  m1;
   char m2;
} aStruct;
#define EXAMPLE3 (*(volatile aStruct *) 0x1000) // A structure @ 0x1000
#define EXAMPLE4 ((volatile aStruct *) 0x1000)  // A ptr to a struct @ 0x1000
aStruct example5 @0x1000; // A structure @ 0x1000
aStruct volatile  *const example6 = ((volatile aStruct *) 0x1000); // A ptr to a struct @ 0x1000
int main(void)
{
   example1 = 0x12345678;
   EXAMPLE2 = 0x12345678;
   EXAMPLE3.m1 = 1234;
   EXAMPLE4->m2 = 'a';
   example5.m1 = 1234;
   example6->m2 = 'b';
     
}
 
It's informative to try dissassembling these in codewarrior to check the code produced.
bye
 
					
				
		
Hello
Notation @ is not standard ANSI C.
So an ANSI C compiler might not support it.
You can submit a Feature request for support of that notation in the compiler through our on-line support web site if you want to see that extension in CodeWarrior some day.
I would recommend you to submit a service request for that.
Click here to submit a service request.
CrasyCat
 
					
				
		
Dear CrazyCat,
I don't understand your comment about the service request.
The example I gave is for the codewarrior CFV2,3,4 compiler so obviously it supports it already  .
. 
The compilers for other targets support this notation as well - They better since they use it in the supplied target header files. However, I note that the header files for the CFV2,3,4 use the pointer casting method.
bye