PUCPAR on MCF52221

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PUCPAR on MCF52221

2,951件の閲覧回数
LPs1978
Contributor III

Hi all,

    I'm trying to set up uart2 on a MCF52221, but in MCF52221_GPIO.h file I cannot find any macro for Port UC. There are macros for PUA and PUB, but nothing referred to PUC.

 

There is something wrong on thereference manual or is only a problem of .h file?

 

Thanks

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,924件の閲覧回数
MrBean
Contributor I

MCF52223 ColdFire® Integrated Microcontroller Reference Manual, Rev. 3

 

12.6.5.2 Quad Function Pin Assignment Registers

Page 12-12

 

The info there is correct.

 

(Use the "Find" (Ctrl+F) function of Adobe Reader!)

 

 

See also: http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=6202

 

 

The PORTUC pins are only available on a 100 pin package.

The MCF52221 is not available in this package according to the Ref Manual.

The website then again says it is available in 100 pins packages.

 

 

Message Edited by MrBean on 2009-03-18 12:23 12:23 PM
0 件の賞賛
返信

1,924件の閲覧回数
LPs1978
Contributor III

Thank you very much. This means that there isn't UART2 on the demo board CPU. :smileyhappy:

0 件の賞賛
返信

1,924件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

On 80 pin devices UART2 is still available as alternative peripheral on port AS.

http://www.utasker.com/forum/index.php?topic=256.0

 

regards

 

Mark

 

 

www.uTasker.com

- OS, TCP/IP stack, USB, device drivers and simulator for M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

 

0 件の賞賛
返信

1,924件の閲覧回数
MrBean
Contributor I

Indeed, and those UART2 pins on PORTAS pins are available on the I/O port connector J1.

No level RS232 converter there. Use an external one if needed.

 

If UART2 is used, you will have to give up on CTS1/RTS1 or move those to PORTQS, giving up on QSPI.

0 件の賞賛
返信