Need help for M5213EVB UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help for M5213EVB UART

1,960件の閲覧回数
Beyond
Contributor I
Dear all,

I am trying to connect a GPS receiver to M5213EVB and using UART on M5213EVB to transmit the GPS data to computer screen. I know I have to initialize the PORTUB (RXD0 and TXD0) and set the baudrate to 4800, 8 data bit, no parity, 1 stop bit, no flow control. I am thinking that I could use on-chip 8MHz oscillator and set PLLMODE to mormal mode, set low power divider as "0000", use system clock as UART clock.
My questions are: How do I set up baud rate? According my setup above, the system clock is 8 MHz, so
do I need to adjust MCF_UART1_UBG1 and UBG2? What exactly are UBG1 and UGB2 register for?

Here is my code for initialization, could someone check it for me, please!

Thanks!!

#include <stdio.h>
#include "mcf5213.h"
#include "common.h"
#include "uart.h"
#include "clock.h"

void Init_CLK(void)
{
 MCF_CLOCK_SYNCR = 0x07;          //set PPLMODE='1',PPLEN='1',CLKsrc='1'
 MCF_CLOCK_LPCR_LPD(4);           //set LPD="0000"
 MCF_PMM_PPMRL = 0x00000040;   //enable UART use system clock   
}

void Init_UART1(void)
{
 uint16 ubgs;
 // assign port pins to UART functions
 MCF_GPIO_PUBPAR = 0 | MCF_GPIO_PUBPAR_TXD1_TXD1 | MCF_GPIO_PUBPAR_RXD1_RXD1;
      
 // Reset Receiver and Transmitter (UCR)
 MCF_UART1_UCR = MCF_UART_UCR_RESET_TX;
 MCF_UART1_UCR = MCF_UART_UCR_RESET_RX;
   
 // Reset Mode Pointer
 MCF_UART1_UCR = MCF_UART_UCR_RESET_MR;
 
 // Initialize Input Enable Control (UACR)
 MCF_UART1_UACR = 0;
   
 // Select Receiver and Transmitter Clock (UCSR)
 
 ubgs = ((8*1000000)/(4800 * 32));

 MCF_UART1_UBG1 = (uint8)((ubgs & 0xFF00) >> 8); //divider MSB
 MCF_UART1_UBG2 = (uint8)(ubgs & 0x00FF);        //divider LSB  
 
 //Set Rx and Tx clocks to system clock
 MCF_UART1_UCSR = 0 | MCF_UART_UCSR_TCS(MCF_UART_UCSR_TCS_SYS_CLK)
                    | MCF_UART_UCSR_RCS(MCF_UART_UCSR_TCS_SYS_CLK);
     
 // Set Mode Register 1 (UMR1)
 MCF_UART1_UMR = 0 // RX Ready will generate interrupt
     | MCF_UART_UMR_BC_8  // 8 bits/char
     | MCF_UART_UMR_PM_NONE;  // no parity
    
 // Set Mode Register 2 (UMR2)
 MCF_UART1_UMR = 0 // normal mode
     | MCF_UART_UMR_SB_STOP_BITS_15; // stop bit width
 
 // Enable Transmitter and Receiver (UCR)
 MCF_UART1_UCR = 0 | MCF_UART_UCR_TX_ENABLED | MCF_UART_UCR_RX_ENABLED;
}
ラベル(1)
0 件の賞賛
返信
1 返信

1,007件の閲覧回数
mjbcswitzerland
Specialist V
Hi Beyond

The registers UBG1 and UBG2 are 2 x 8 bit registers which are combinded into one 16 bit divider value.

As an example, to set 19'200 BAUD the following can be used:

unsigned short  usSpeed = (BUS_CLOCK/32 + 19200/2)/19200;                        // set 19200
UBG1 = (unsigned char)(usSpeed >> 8);
UBG2 = (unsigned char)(usSpeed);

Regards

Mark Butcher

www.uTasker.com

0 件の賞賛
返信