Missing Interrupt Sources Table in MCF52235 Reference Manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing Interrupt Sources Table in MCF52235 Reference Manual

1,489 Views
RValls
Contributor III

Hi!

I have "updated" my copy of the reference manual (which was Rev.4) to the lattest available in the website (which is Rev.7) and I have found that the Interrupt Sources Table (which was Table 15-6) is missing. In fact, In section "15.3.8.1 Interrupt Sources", it actually says

"Table 15-6 lists the interrupt sources for each interrupt request line."

and table 15-6 is not the Interrupt Sources table.

 

Is it actually a mistake of the revision or they have moved it to another place and I haven't found it?

Can somebody upload an ancient Rev. of the manual which has got this table?

And how to report this to Freescale?

 

Best regards,

Rubén

Labels (1)
0 Kudos
Reply
2 Replies

1,312 Views
TomE
Specialist II

Documentation bug.

 

Found last July and reported to Freescale. They released an Addendum to the manual in December and didn't include this information. I've reported it as well. Don't expect it to be fixed any time soon.

 

Refer to the following link for details on where to read the missing pages on line:

 

https://community.freescale.com/thread/109270

 

Tom

 

0 Kudos
Reply

1,312 Views
RValls
Contributor III

Thank you very much Tom!

 

It is also interesting the discussion on interrupt sources that carries the thread, because I'm also using the Interniche Stack, and also have the same bugs.

 

Thank you again,

Best regards,

Ruben

0 Kudos
Reply