Memory use of uTasker and SSL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory use of uTasker and SSL

1,299件の閲覧回数
paul1962
Contributor I

Hi,

 

I have a use for a TCP/IP stack which supports SSL/TLS and wondered if anyone was using the uTasker system and could give some idea of memory use - code and ram etc.

My target is the MCF53014.

 

If anyone has any other recommendations for tcp/ip with tls which will run either without an operating system or come with its own o/s please let me know.

I have limited memory on the target board, basically just the 128K of ram built into the 53014 and 1megabyte of flash so small memory use is a must!

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,252件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Do you mind to put your question on the uTasker forum instead:

µTasker Forum - Index 

0 件の賞賛
返信