MKV56F512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,060件の閲覧回数
jian3_wang
Contributor I

Q1: Can the VDDA be powered before VDD?

Q2: Can the VREFH voltage be powered before VDD and VDDA?

thanks

1 解決策
1,922件の閲覧回数
TomE
Specialist II

MKV56F512 is a Kinetis part. This forum is for Coldfire parts. You should MOVE the question to that Forum (there's an option for this if you're the Author of a post, but the addition of my post might interfere with that).

The Reference Manual says "V REFH must never exceed V DDA".

You should also read "40.7.1.1 Analog supply pins". It is quite clear on the matter.

Tom

元の投稿で解決策を見る

2 返答(返信)
1,923件の閲覧回数
TomE
Specialist II

MKV56F512 is a Kinetis part. This forum is for Coldfire parts. You should MOVE the question to that Forum (there's an option for this if you're the Author of a post, but the addition of my post might interfere with that).

The Reference Manual says "V REFH must never exceed V DDA".

You should also read "40.7.1.1 Analog supply pins". It is quite clear on the matter.

Tom

1,922件の閲覧回数
jian3_wang
Contributor I

Thanks for your information.

0 件の賞賛
返信