> when i execute the stop commmand nothing happens
Isn't "nothing" exactly what is meant to happen when you execute "stop"? :smileyhappy:
Are you running it with a debugger attached? That may be affecting what you see.
"STOP" has a parameter - the new CPU Status Register contents. The usual way to use STOP is to disable all interrupts (set the SR to 0x2700), then do any setup/wakeup stuff then execute the STOP with the IPL that you have set up to wake the CPU up again. To wake up with all interrupts this is "0x2000", to set to CPU to IPL "n" it is "0x2n00.
I assume you have a timer running or have it set up to interrupt on an external pin. Maybe a different interrupt is happening to the one you expect. Maybe a timer is running or a serial port is interrupting?
Tom