MCG Configuration, Handling An Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCG Configuration, Handling An Error

1,691件の閲覧回数
R_R_Ritchey
Contributor II

I have a project where I need to keep the processor going even if the MCG configuration fails at some point in going from FEI to PEE.  When I exit the clock configuration the processor clock needs to be 48MHz whether its referenced from the external crystal or the internal clock (trimmed to 31.250 KHz).  I am at the point where I needed to figure out how to handle a failure going from FEI -> FBE -> PBE -> PEE at any point to get back to FEI.  Obvious way is to backtrack but wondered if there was an easier way to get back to FEI from any point further in the chain. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,560件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Does your issue been address with this post: https://community.nxp.com/thread/456183 

0 件の賞賛
返信