MCF5485 FEC inverted CRC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5485 FEC inverted CRC

2,914件の閲覧回数
alexeyminkov
Contributor I

Good afternoon. Information on MCF5485.

 

FEC0 through MII is connected to the transmitter KSZ8051 next is plug on itself.

 

Did initialization FEC0 below is attached.

Made a simple program written in the FIFO and the reader.

Look at the results, the data came, and on a bad CRC.

The coup is at the stage of issuance.

How to get rid of this?

I.e. If I have a personal computer, give the package, everything is fine.

And when trying to transfer from the PC, the FEC0 CRC error.

In p. "31.4.2.2 Transmit Frame Control Word (TFCW) indicates that the 1 Transmit the CRC sequence inverted after the last data bye (regardless of the TC value)» how to get rid of this?


   move.l  #0x80009024,a1        //#ECR0    Сброс всех регистров FEC0
             move.l  #0x00000001,(a1)
             nop
             nop
        
             move.l  #0x80009008,a1   //#EIMR0
             move.l  #0x00000000,(a1)   //Запретить все прерывания fec0
           
             move.l  #0x80009004,a1                     //#EIR0    Очистить регистр прерываний FEC0
             move.l  #0xffffffff,(a1)
     
           
             move.l  #0x80009144,a1   //#FECTFWR0 Настроить Watermark: кол-во байт в FIFO, после 
             move.l  #0x7,(a1)   //которого начнется передача (512)=64*(7+1)
           
             move.l  #0x80009118,a1   //#IAUR0    Индив.адр.назначения
             move.l  #0x0,(a1)   //Старшие 32 разряда
           
             move.l  #0x8000911c,a1   //IALR0    Младшие 32 разряда
             move.l  #0x0,(a1)
           
             move.l  #0x80009120,a1   //#GAUR0    Групп.адр.назначения
             move.l  #0x0,(a1)   //Старшие 32 разряда

 

             move.l  #0x80009124,a1   //#GALR0    Младшие 32 разряда

 

             move.l  #0x0,(a1)
           
             move.l  #0x800090e4,a1   //#PALR0    Физический адр.назначения
             move.l  #0x0,(a1)   //Младшие 32 разряда
           
             move.l  #0x800090e8,a1   //#PAHR0    Старшие 16 разрядов
             move.l  #0x8808,(a1)
           
             move.l  #0x80009084,a1   //#RCR0   Receive Ctrl: max frame lenght=1518 (0x5ee)
             move.l  #0x05ee000c,(a1)         //PROM=1 (all frames); MII_MODE=1

 

             move.l  #0x800090c4,a1   //#TCR0   Transmit Ctrl: full duplex enable
             move.l  #0x4,(a1)
                           
             move.l  #0x80009064,a1   //#MIBC0    MIB logic halt
             move.l  #0xc0000000,(a1)
           
             move.l  #0x80009200,a1   //#RMON_T_DROP0    Инициализация счетчиков
fe10:           
             move.l  #0x00000000,(a1)+
             cmpa.l  #0x80009278,a1
             bne fe10
           
             move.l  #0x80009280,a1   //#RMON_R_DROP0
fe20:           
             move.l  #0x00000000,(a1)+
             cmpa.l  #0x800092e4,a1
             bne fe20
           
             move.l  #0x80009064,a1   //#MIBC0    MIB logic enable
             move.l  #0x00000000,(a1)
                
             move.l  #0x800091c4,a1   //#FECFRST0    Reset FIFOs
             move.l  #0x03000000,(a1)
             move.l  #0x00000000,(a1)
             nop
             nop
             nop

 

             move.l  #0x800091ac,a1   //#FECTFCR0    Transmit: Frame mode enable;
             move.l  #0x09340000,(a1)         //last transfer granularity = 1; FIFO underflow mask

 

             move.l  #0x8000918c,a1   //#FECRFCR0 Receive: аналогично transmit
             move.l  #0x09140000,(a1)
           
             move.l  #0x800091c8,a1   //#FECCTCWR0    CRC enable
             move.l  #0x03000000,(a1)
           
             move.l  #0x800091b8,a1   //#FECTFAR0    Trans Alarm - 1023
             move.l  #0x200,(a1)//512
           
             move.l  #0x80009198,a1   //#FECRFAR0    R Alarm - уст.,когда осталось 768 байт
             move.l  #0x200,(a1)//512

 

             move.l  #0x80009024,a1
             move.l  #0x00000002,(a1)           
  
             move.l  #0x80009044,a1
             move.l  #0x000000B0, (a1)
  
             move.l  #0x80009040,a1   //4
             move.l  #0x509201E1, (a1)
           
             move.l  #0x80009040,a1   //1
             move.l  #0x50822100, (a1)
ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,580件の閲覧回数
TomE
Specialist II

I think your mistake is this:

move.l    #0x800091c8, a1       //#FECCTCWR0  CRC enable

move.l    #0x03000000, (a1)

"CRC Enable" is 0x02000000 and not 0x03000000

You're also setting the TFCW (Transmit Frame Control Word Enable) bit, which is telling the transmitter to read an EXTRA 32-bits from the FIFO. One of the bits in that extra word is "transmit the wrong CRC". Don't set the TFCW bit in the first register and it shouldn't transmit the bad CRC.

Tom

0 件の賞賛
返信

2,580件の閲覧回数
TomE
Specialist II

The Ethernet controller in the MCF5485 looks to be a derivative of the one in the MPC5200.


There is driver code here for that chip:

http://lxr.free-electrons.com/source/drivers/net/ethernet/freescale/

However, the MPC5200 uses a very complicated "Bestcom" DMA controller, which looks to be different to the one in the MCF5485.

The MPC5200 manual documents a "Table 14-38. FEC Transmit FSM Register" which is similar to the "31.3.3.35 FEC CRC and Transmit Frame Control Word Register (FECCTC)" one in the MCF5485. In the MPC part the register enables (separately) Generating and Appending the CRC. It looks like the "14.9.3.2 Transmit Frame Control Word" is compulsory for this chip, and that controls on a per-frame basis whether the CRC is transmitted, and if it is good or bad. In the MCF5485 it looks like the FECCTC register controls whether the TFCW is to be used, so it seems to be optional.

If the manual is wrong and it isn't optional, you need to (somehow) send a valid TFCS as part of the transmit stream.

Why are you writing in assembly? If you wrote in C you should at least have header files defining the registers and the contents already available.

Tom

2,580件の閲覧回数
alexeyminkov
Contributor I
Thank you very much Tom Evans.

I figured out.

To record the "WFR bit"/"WCTL bit" registry FEC "the Transmit FIFO Control Register (FECTFCR)" and then write "data"/"Control Word".

Now everything works.

0 件の賞賛
返信