what is the resistor value on the MCF52259's reset state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the resistor value on the MCF52259's reset state

892件の閲覧回数
junhu
Contributor I

if MCF52259 enter a reset state, its datasheet said "All signals have a pull-up in GPIO mode". my question is: what the resistor value is?

ラベル(1)
0 件の賞賛
返信
1 返信

793件の閲覧回数
TomE
Specialist II

> what the resistor value is?

That isn't in the Reference Manual. It is an electrical characteristic of the chip, so it is in the Data Sheet.


Specifically "Table 13. DC Electrical Specifications":

    Weak internal pull Up device current, tested at VIL Max.  -10 to -130 uA.

The "pullup" may not be a linear resistor, but may be a current source. Given the above currents, it is somewhere between 25k and 330k measured to ground.

Tom