MCF547x/548x files missing from bitshrine?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF547x/548x files missing from bitshrine?

2,747 Views
aeg
Contributor I
Hi guys,

I just downloaded the latest ltib from savannah but noticed that the MCF547x/548x uses a lot of files not yet published on bitshrine....?

Is there another way to get these patches for 2.6.24?

Thanks,
Andreas

Here are the patches needed:

#
Patch47 : lin2-6-24-m5445x-kbuild.patch
Patch48 : lin2-6-24-m5445x-usb-header-fix.patch
Patch49 : lin2-6-24-m5445x-lock-header.patch
Patch50 : lin2-6-24-m5445x-pata-struct.patch
Patch51 : lin2-6-24-m5445x-remove-cdev.patch
#
Patch52 : linux-2.6.24-m547x_8x-548x-headers.patch
Patch53 : linux-2.6.24-m547x_8x-initial.patch
Patch54 : linux-2.6.24-m547x_8x-serial.patch
Patch55 : linux-2.6.24-m547x_8x-init-defconfig.patch
Patch56 : linux-2.6.24-m547x_8x-dma.patch
Patch57 : linux-2.6.24-m547x_8x-fec.patch
Patch58 : linux-2.6.24-m547x_8x-fec-cleanup.patch
Patch59 : linux-2.6.24-m547x_8x-dma-cleanup.patch
Patch60 : linux-2.6.24-m547x_8x-xtra-disable.patch
Patch61 : linux-2.6.24-m547x_8x-cache.patch
Patch62 : linux-2.6.24-m547x_8x-kernphys.patch
Patch63 : linux-2.6.24-m547x_8x-uboot.patch
Patch64 : linux-2.6.24-m547x_8x-phys-defconfig.patch
Patch65 : linux-2.6.24-m547x_8x-fec-remove-debug.patch
Labels (1)
0 Kudos
Reply
3 Replies

1,751 Views
kmahan
Contributor I
Hi Andreas,

We will be pushing these files to bitshrine in the next week or so -- I'll post a response when they are available.

Please note that this version is NOT supported by Freescale.  The kernel spec file is part of an upcoming release that is not finished.  It is expected that there will be changes between now and the final release.

Supported releases are available in the BSPs downloadable from Freescale.

--Kurt
0 Kudos
Reply

1,751 Views
comio
Contributor I
This a great news...


luigi
0 Kudos
Reply

1,751 Views
aeg
Contributor I
Hi Kurt,

and thanks for doing this.
I am aware of the lack of official support and will report any findings back to the community.

Do you have an idea of what 547x_8x are weak in this version? What works well? Any info is always helpful.
Finally, when would an official ISO release be expected?

Thanks again and feel free to ping me anytime for status reports etc etc.

-A


0 Kudos
Reply