MCF5445x, On-Chip USB Transceiver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5445x, On-Chip USB Transceiver

1,352 Views
KyleFromBullex
Contributor III

Hello everyone,

 

I'm bringing up a custom board with two 54450 processors, both of which use the built-in FS/LS USB transceiver. I'm using a slightly modified Freescale Linux kernel with support for the FS/LS transceiver enabled, and the internal PLL used rather than the external USB clock. One of the processors is connected to a USB hub, and the other is wired directly to an external USB port.

 

So far, I haven't been able to get any signal out of either processor. I've tried putting the USB port in test mode, to no avail. This may be because the internal transceiver doesn't support HS, which according to section 7.1.20 of the USB 2.0 standard means it doesn't support test mode. The driver starts up fine, but it doesn't detect the onboard USB hub.

 

Could somebody please help me out here? From what I understand, the FS/LS transceiver is supposed to make USB simple to implement. Is there a known issue with the Freescale USB Linux drivers that could be causing this? Thanks in advance.

 

Kyle

Labels (1)
0 Kudos
Reply
1 Reply

1,155 Views
KyleFromBullex
Contributor III

Sorry guys, I probably should have mentioned that we're operating solely in host mode for both processors.

0 Kudos
Reply