MCF54450 V4e SRAM performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF54450 V4e SRAM performance

ソリューションへジャンプ
3,723件の閲覧回数
SMRSteve
Contributor II

Hello all.

 

I'm working on a rather software-intensive application (video encoder) at the moment, and am trying everything possible to optimise my code. I have discovered that the on-board 32kB SRAM does not seem to be as fast as it should be:

 

After writing some simple data-copying benchmarks, I have the following results:

 

DDR to DDR copy = 40.8 MB/s (copyback mode)

DDR to DDR copy = 79.2 MB/s (write-through mode)

SRAM to SRAM copy = 129.6 MB/s

Cache to cache copy = 399.2 MB/s

 

(Platform is MCF54450 at 240MHz with mobile-DDR external memory. Copies run with simple MOVEM loops - not DMA)

 

Now, the datasheet says the SRAM is single-cycle and on the processor's local high-speed bus. Should this not therefore give a bandwidth of 960MB/s, or copy performance of 480MB/s for 32-bit wide memory? I'm getting this sort of speed from the cache, but the SRAM seems far too slow. If the SRAM is this slow, what's the point of it? Code or data structures will always be faster in cached external memory.

 

I have played about with the RAMBAR settings, and am accessing the SRAM properly - not through the backdoor!

 

Thanks for any advice!

 

Steve.

 

PS. If anyone's interested in my benchmarking routines, let me know and I'll post them.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,882件の閲覧回数
SMRSteve
Contributor II

I've now found the solution to this one;

 

First, I must thank TomE for prompting me to double-check the RAMBAR to make sure I wasn't accessing through the backdoor. I tried to get a backdoor access benchmark for comparison, and it came out the same speed. Long story short, my assembler is writing $C04 instead of $C05 for the RAMBAR, so after looking up the MOVEC opcode, I now have reasonable SRAM performance:

 

SRAM to SRAM copy (backdoor) = 129.6 MB/s

SRAM to SRAM copy (direct) = 351.6 MB/s
Cache to cache copy = 399.2 MB/s

 

So, still not quite as fast as the cache, but I now see no performance difference in my application code whether I use SRAM or cached DDR for the data.

 

Steve.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,882件の閲覧回数
TomE
Specialist II

Me again. I suggested checking the RAMBAR settings in your other post on optimisation before reading this one.

 

Concerning memory speed. I'm using a 240MHz MPC5329. It is documented (but not well) as having a maximum memory bandwidth of 128MB/s with an 80MHz SDRAM clock. I can't get anything (even DMA) running at that speed.

 

That throughput assumes burst reads or writes to and from SDR or DDR. The memory controller is limited to taking 10 clocks to issue Precharce, Bank Select and then four Reads (four 32-bit reads for SDN, 8 double-clock 16-bit reads at exactly the same data rate for DDR). Except I'm measuring 11 clocks instead of 10, and neither the CPU or DMA can keep up with it.

 

The SDRAM controller will NOT hold banks open, and insists on taking 6 clocks on precharge and bank-select, even between bursts to successive memory addresses. It looks like the V4 one does the same.

 

https://community.freescale.com/thread/59655

 

The only instructions in the V3 Coldfire that can WRITE to memory in a four-clock burst are the MOVEM.L ones. Normal Moves seem to write one word at a time, non-bursting. I see you're using these already.

 

https://community.freescale.com/message/60698#60698

 

These are copy speeds, double them to get bandwidth figures.

 

 

Function       Four runs in microseconds  Average  Stdev  MB/s   Theorymemcpy            4369  4310  4312  4308  4324.75  29.55  38.85  60.70%memcpy_gcc_2      4399  4400  4399  4399  4399.25  0.5    38.19  59.67%memcpy_gcc_4_3    4439  4439  4438  4439  4438.75  0.5    37.85  59.14%memcpy_gcc_4_4    4833  4831  4832  4832  4832     0.82   34.77  54.33%memcpy_moveml     3625  3625  3625  3625  3625     0      46.34  72.41%

You're getting 79MB/s. If that's the copy rate then you're getting double what I'm getting. If you're quoting "bandwidth" then you're slower than I am with movem.l. I think you're running the memory at 120MHz so you should be 1.5 times faster than the V3 core at 80MHz.

 

 

Make sure your source and destination buffers are 16-byte aligned.

 

The problem with the "copyback" is that it has to READ the destination cache line before you then overwrite ALL of it, so the copy runs at 1/3 of the bandwidth (read, read, write). A Writethrough runs at 1/2 (read, write). What would be nice to do in your copy if you want to use copyback would be to invalidate the cache line before writing to it. The PPC core has instructions for this, but the Coldfire doesn't.

 

I don't know why your copyback is running at 1/2 of your writethrough speed though. is this as you expect?

 

0 件の賞賛
返信
2,882件の閲覧回数
SMRSteve
Contributor II

Hello TomE,

 

The figure of 79 MB/s is a copy speed. If I benchmark read, write, and copy separately I get these figures:

 

Read = 136.7 MB/s

Write = 254.5 MB/s

Copy = 79.3 MB/s

 

This is with mobile-DDR clocked at 120MHz (16-bit wide).

 

Based on your figure of 10 clocks minimum for a 16-byte transfer, I make the maximum to be 192 MB/s. I can't find any timing diagrams in the datasheet, but it has to be less than 10 clocks to be able to get a write speed of 254 MB/s, in fact, no more than 7.5 clocks.

 

I'm starting to doubt my benchmark is correct now, although I can't see anything wrong. The code is thus:

 

        move.l   #65536,d1                                      ;number of 16-byte bursts to do (= 1MB)

        moveq.l #64,d0                                            ;constant to add to address

        movea.l #SDRAM_SCRATCH,a0            ;somewhere to write to

        move.w  #$2700,SR                                    ;no interruptions please

        move.l   DTCN0,d7                                      ;start the clock

loop

        subq.l  #4,d1                                                 ;dec loop counter (4 bursts) & update CCR

        movem.l d2-d5,(a0)                                     ;burst write

        movem.l d2-d5,16(a0)

        movem.l d2-d5,32(a0)

        movem.l d2-d5,48(a0)

        adda.l   d0,a0                                                ;advance address

        bgt.s   loop                                                     ;CCR from subq earlier

        move.l   DTCN0,d0                                      ;stop the clock

        move.w  #$2000,SR

        sub.l   d7,d0                                                  ;subtract start clock, d0 = microseconds to write 1MB

        move.l  #1000000000,d1                           ;(one billion)

        divu.l  d0,d1                                                  ;d1 is kB/s (or MB/s to 3 d.p.)

 

DTCN0 is free-running at 1MHz. I know this is right as it's used by the OS for generating delays. As you can see, I am just writing whatever garbage is in d2-d5, but that's not the point - it's a memory speed test.

 

Maybe I should write a DMA speed test - presumably that would give me the absolute memory speed as there'll be no instructions to slow it down.,,

 

As for the copyback, 1/2 the speed sounds right to me for a straight copy routine, as the CPU stalls while the cache writes the old line out before it can accept a new line. In write-through mode the write to DDR and the write to cache are done at the same time. I couldn't say whether it should be 1/2 the speed, or 1/3 of the speed, but I'm not surprised by the figures I'm getting.

 

Steve.

 

0 件の賞賛
返信
2,882件の閲覧回数
TomE
Specialist II

> Based on your figure of 10 clocks minimum for a 16-byte transfer

 

That's for the V3 SDRAM controller. The V4 one looks to be better. It has:

 

- Supports page mode for decreased latency and higher bandwidth; remembers

- one active row for each bank; four independent active rows per each chip select

 

If you can get your read and write addresses in different BANKS it should go faster. The worst thing would be alternating short (non-cache-line or single-cache-line length) reads and writes in the same bank. Maybe your writeback memory test is doing that (flush a line, read a line) where your writethrough test can get longer bursts.

 

> Maybe I should write a DMA speed test - presumably that would give me

> the absolute memory speed as there'll be no instructions to slow it down.,,

 

I found the V3 DMA to be as slow as the CPU. Monitoring the memory bus with a CRO showed that after the burst read and write the DMA controler just stalled. My guess is that it isn't pipelined and took multiple clocks to do something, presumably to add the offsets to the source and destination addresses and to decrement and test the counter.

 

0 件の賞賛
返信
2,882件の閲覧回数
SMRSteve
Contributor II

Good point about putting the read and write in different banks:

 

Copy (same bank) = 79.3 MB/s

Copy (different banks) = 89.5 MB/s

 

I tried the DMA copy too, with disappointing results:

 

Copy (DMA, different banks) = 62.8 MB/s

 

Steve.

 

0 件の賞賛
返信
2,883件の閲覧回数
SMRSteve
Contributor II

I've now found the solution to this one;

 

First, I must thank TomE for prompting me to double-check the RAMBAR to make sure I wasn't accessing through the backdoor. I tried to get a backdoor access benchmark for comparison, and it came out the same speed. Long story short, my assembler is writing $C04 instead of $C05 for the RAMBAR, so after looking up the MOVEC opcode, I now have reasonable SRAM performance:

 

SRAM to SRAM copy (backdoor) = 129.6 MB/s

SRAM to SRAM copy (direct) = 351.6 MB/s
Cache to cache copy = 399.2 MB/s

 

So, still not quite as fast as the cache, but I now see no performance difference in my application code whether I use SRAM or cached DDR for the data.

 

Steve.

0 件の賞賛
返信