MCF54415 usb host stack

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCF54415 usb host stack

跳至解决方案
1,751 次查看
dmitrytrefilov
Contributor I

Hi! I was planning to use in one of my projects Coldfire V4 MCF54415 processor. I had a few questions:

1) Where can I find USB Host Stack for this processor?

2) If he does not exist, how can I write own USB Stack?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,562 次查看
yibbidy
Contributor V

If you are using an RTOS then you could ask your vendor.  If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP .  The MCF54415 is supported on the current release which is V4.2.

Good luck with your project.

Regards, Shaun

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,563 次查看
yibbidy
Contributor V

If you are using an RTOS then you could ask your vendor.  If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP .  The MCF54415 is supported on the current release which is V4.2.

Good luck with your project.

Regards, Shaun

0 项奖励
回复