MCF54415 usb host stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF54415 usb host stack

Jump to solution
1,700 Views
dmitrytrefilov
Contributor I

Hi! I was planning to use in one of my projects Coldfire V4 MCF54415 processor. I had a few questions:

1) Where can I find USB Host Stack for this processor?

2) If he does not exist, how can I write own USB Stack?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,511 Views
yibbidy
Contributor V

If you are using an RTOS then you could ask your vendor.  If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP .  The MCF54415 is supported on the current release which is V4.2.

Good luck with your project.

Regards, Shaun

View solution in original post

0 Kudos
Reply
1 Reply
1,512 Views
yibbidy
Contributor V

If you are using an RTOS then you could ask your vendor.  If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP .  The MCF54415 is supported on the current release which is V4.2.

Good luck with your project.

Regards, Shaun

0 Kudos
Reply