MCF54415 usb host stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF54415 usb host stack

ソリューションへジャンプ
1,666件の閲覧回数
dmitrytrefilov
Contributor I

Hi! I was planning to use in one of my projects Coldfire V4 MCF54415 processor. I had a few questions:

1) Where can I find USB Host Stack for this processor?

2) If he does not exist, how can I write own USB Stack?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,477件の閲覧回数
yibbidy
Contributor V

If you are using an RTOS then you could ask your vendor.  If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP .  The MCF54415 is supported on the current release which is V4.2.

Good luck with your project.

Regards, Shaun

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,478件の閲覧回数
yibbidy
Contributor V

If you are using an RTOS then you could ask your vendor.  If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP .  The MCF54415 is supported on the current release which is V4.2.

Good luck with your project.

Regards, Shaun

0 件の賞賛
返信