MCF54415 boot from NorFlash failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF54415 boot from NorFlash failed

1,326 Views
changliu1
Contributor I

We are using MCF54415 with BDM mode.

The mcf54415 boot from  a 4M_8bits_NorFlash.

I have modified the *.lcf to make almost all  .code segment ,.data segment and .bss segment  in ROM mode as the same as in RAM mode.

In ROM mode , the board can startup OK, copy all codes / data to the right address and clear the .bss segment.

Now all my codes are running OK in RAM mode, but when in ROM mode , the board failed.

In ROM mode, a task of CAN communication timed out. In RAM mode , use the same codes, the CAN task will not time out.  

I want to know why the same code running  different results in RAM and ROM mode.

Original Attachment has been moved to: RAM_ROM_xMAP.rar

0 Kudos
Reply
1 Reply

1,185 Views
miduo
NXP Employee
NXP Employee

Hi,

Do you interface the NOR flash with the Flexbus? The booting process from FlexBus should be automatic depending on the BOOTMOD[1:0] pins. When they are 0:0, it boots from flexbus with default configuration, but with this configuration, the port size is 8bit. Therefore you need to configure the BOOTMOD[1:0] = 01. And use the FB:AD[7:0] pins to configure the boot configurations.

0 Kudos
Reply