MCF5407 UART interrupt masks seem inverted

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5407 UART interrupt masks seem inverted

3,091件の閲覧回数
jbolduc
Contributor I

Hi, I am having a lot of trouble configuring the UART on the MCF5407. The only way I was able to make the UART work with the interrupt is to inverse the UIMR bit logic; the datasheet says that we must set TxRDY and FFULL so the interrupts can be asserted but for me, it's the opposite.

I must clear FFULL for Rx, and clear TxRDY when sending and set when software tx fifo is empty.

I copied the problematic code below. To make it work for me, I must inverse ENABLE and DISABLE in the main loop and in HandleUart(void).

When I try to transfer this code to the main project, we have interrupt issues. There is something wrong that I can't figure out.

Thanks for the help

#include "mcf5407.h"
#include "CpuReg.h"
#include "FifoBuffer.hpp"

#define ENABLE TRUE
#define DISABLE FALSE

#define CPU_CLOCK_FREQ_HZ 54000000 // 54 MHz for NGDU

#define VECTOR_TABLE 0x00000000

#define UART0_ICR MCF5407_SIM_ICR4

void Hardware_Init();
void SetSR( UINT32 sr );
UINT32 GetSR();

static unsigned char g_rxBuffer[256];
static FifoBuffer<unsigned char> g_rxFifo(g_rxBuffer, 256);

static unsigned char g_txBuffer[256];
static FifoBuffer<unsigned char> g_txFifo(g_txBuffer, 256);

typedef enum
{
 SERIAL_CMD_NONE = 0x00, // no command - ignored
 SERIAL_CMD_RESET_MRP = 0x01, // reset mode register pointer
 SERIAL_CMD_RX_RESET = 0x02, // reset the receiver
 SERIAL_CMD_TX_RESET = 0x03, // reset the transmitter
 SERIAL_CMD_RST_ERR_STAT = 0x04, // reset the receiver
 SERIAL_CMD_RESET_BCI = 0x05, // reset break change interrupt
 SERIAL_CMD_START_BREAK = 0x06, // start a break
 SERIAL_CMD_STOP_BREAK = 0x07 // stop break
} SERIAL_CMD;

void SendCommand(SERIAL_CMD enCmd)
{
 uint8 cmd = ((UINT8)enCmd & 0x07)<<4;
 CPU_WR(MCF5407_UART0_UCR, cmd);
}

void SetBaudrate()
{
 UINT16 divisor = ROUND32(CPU_CLOCK_FREQ_HZ / 32.0f / 19200 ); // SERIAL_19K2_BAUD

 CPU_WR(MCF5407_UART0_UCSR, 0xDD); // Use prescaled CLKIN for tx/rx
 CPU_WR(MCF5407_UART0_UBG2, (UINT8)divisor); // Lower byte of divisor
 CPU_WR(MCF5407_UART0_UBG1, (UINT8)(divisor >> 8)); // Upper byte of the divisor
}

void Transmitter(BOOL bEnable)
{
 UINT8 bitCode = bEnable ? (0x01 << 2) : (0x02 << 2);
 CPU_WR(MCF5407_UART0_UCR, bitCode);
}

void Receiver(BOOL bEnable)
{
 UINT8 bitCode = bEnable ? 0x01 : 0x02;
 CPU_WR(MCF5407_UART0_UCR, bitCode);
}

void ReceiverInterrupts(BOOL bEnable)
{
 volatile UINT8 status = CPU_RD(MCF5407_UART0_UIMR);
 if (bEnable) {
 status |= MCF5407_UART_UIMR_FFULL; // Enable
 } else {
 status &= ~MCF5407_UART_UIMR_FFULL; // Disable
 }
 CPU_WR(MCF5407_UART0_UIMR, status);
}

void TransmitterInterrupts(BOOL bEnable)
{
 volatile UINT8 status = CPU_RD(MCF5407_UART0_UIMR);
 if (bEnable) {
 status |= MCF5407_UART_UIMR_TXRDY; // Enable
 } else {
 status &= ~MCF5407_UART_UIMR_TXRDY; // Disable
 }

 CPU_WR(MCF5407_UART0_UIMR, status);
}

void SetInterruptMask(BOOL bSet)
{
 UINT32 mask = CPU_RD32(MCF5407_SIM_IMR);
 if (bSet) {
 mask |= MCF5407_SIM_IMR_UART0;
 } else {
 mask &= ~MCF5407_SIM_IMR_UART0;
 }
 CPU_WR32(MCF5407_SIM_IMR, mask);
}

#define ANY_UART_ERRORS (MCF5407_UART_USR_RB | \
 MCF5407_UART_USR_FE | \
 MCF5407_UART_USR_PE | \
 MCF5407_UART_USR_OE)

void HandleUart(void)
{
 int maxRead = 4;

 volatile uint8 uisr = CPU_RD(MCF5407_UART0_UISR);
 // RX INTERRUPT
 if (uisr & (MCF5407_UART_UIMR_FFULL))
 {
 volatile uint8 usr = CPU_RD(MCF5407_UART0_USR);
 //while FIFO is not empty?
 while (usr & (MCF5407_UART_USR_RXRDY) && (maxRead--) > 0)
 { 
 if (usr & ANY_UART_ERRORS)
 {
 SendCommand(SERIAL_CMD_RST_ERR_STAT);
 }
 g_rxFifo.Insert(CPU_RD(MCF5407_UART0_URB));
 usr = CPU_RD(MCF5407_UART0_USR);
 }
 }

 // TX INTERRUPT
 if (uisr & (MCF5407_UART_UIMR_TXRDY))
 {
 if (g_txFifo.GetCurrentLength() > 0)
 {
 volatile UINT8 usr = CPU_RD(MCF5407_UART0_USR);
 // determine if this buffer descriptor is ready to be loaded 
 if (usr & MCF5407_UART_USR_TXRDY) { // TX Ready Bit Set
 UINT8 byte = g_txFifo.Extract();
 CPU_WR(MCF5407_UART0_UTB, byte);
 }
 }

 }

 if (g_txFifo.IsEmpty())
 {
 TransmitterInterrupts(DISABLE);
 }
}

__declspec( interrupt ) void UartIntHandler(void)
{
 HandleUart();
}

void InstallHandler()
{
 UINT32 *vt = (UINT32 *)(VECTOR_TABLE);
 // Autovector isr 1-7 --> vector number 25-31 (UINT32)
 // isr level 6 == vector 30
 vt[ 30 ] = (UINT32)UartIntHandler;
}

void InitUart()
{
 Receiver(DISABLE);
 Transmitter(DISABLE);
 
 ReceiverInterrupts(DISABLE);
 
 SetInterruptMask(TRUE);
 
 InstallHandler();

 SendCommand(SERIAL_CMD_RX_RESET);
 SendCommand(SERIAL_CMD_TX_RESET);
 
 SendCommand(SERIAL_CMD_RESET_MRP);
 
 CPU_WR(MCF5407_UART0_UACR, 0);
 
 SetBaudrate();

 volatile UINT8 mrp1 = (0x0 << 7) | (0x0 << 6) | (0x1 << 5) | (0x4 << 2) | (0x3 << 0);
 volatile UINT8 mrp2 = (0x0 << 6) | (0x0 << 5) | (0x0 << 4) | (0x7 << 0);
 
 CPU_WR(MCF5407_UART0_UMR, mrp1);
 CPU_WR(MCF5407_UART0_UMR, mrp2);
 
 SendCommand(SERIAL_CMD_RST_ERR_STAT); //reset error status
 SendCommand(SERIAL_CMD_RESET_BCI); //reset break-change interrupt

 UINT8 intLevel = 6;
 UINT8 intPrio = 3;
 UINT8 icrValue = (MCF5407_SIM_ICR_AVEC) | MCF5407_SIM_ICR_IL(intLevel) | (intPrio);
 // Set up the interrupt level and priority
 CPU_WR( UART0_ICR, icrValue );

 SetInterruptMask(FALSE);

 ReceiverInterrupts(ENABLE);
 TransmitterInterrupts(DISABLE);
 
 Receiver(ENABLE);
 Transmitter(ENABLE);
}

int main()
{
 Hardware_Init();
 InitUart();
 
 ReceiverInterrupts(ENABLE);

 while (1)
 {
 if (g_rxFifo.GetCurrentLength() > 0)
 {
 while (!g_rxFifo.IsEmpty() && g_txFifo.GetFree() >= 1)
 {
 g_txFifo.Insert(g_rxFifo.Extract());
 }
 TransmitterInterrupts(ENABLE);
 }
 }

 return 0;
}

void Hardware_Init()
{
 //-------------------------------------------------------------------------
 // Out of reset, only level 7 interrupts are enabled. Enable down to
 // level 3 interrupts (Timer and UART interrupts are enabled)
 //-------------------------------------------------------------------------
 SetSR( 0x2200 );

}

/*-----------------------------------------------------------------------------
| Title: Set CPU Status Register (SR) Value
\*---------------------------------------------------------------------------*/
void SetSR( UINT32 sr )
{
asm {
 move.w d0,sr
 nop
 }
}


/*-----------------------------------------------------------------------------
| Title: Get CPU Status Register (SR) Value
\*---------------------------------------------------------------------------*/
UINT32 GetSR()
{
asm {
 move.w sr,d0
 nop
 }
}

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,931件の閲覧回数
TomE
Specialist II

There should be some linux serial drivers for this hardware. Google might be able to find you some sources. They certainly aren't in the current distributions.

I found references to there being sources in the ucLinux sources here (reference, not the sources) under "Interrupt-based driver for Wacom Artpad":

My life with the MCF5407 Coldfire Board \\ (draft) 

There might be something in here:

http://en.verysource.com/item/dbug_rar-152755.html 

Tom

0 件の賞賛
返信

2,931件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

MCF5407 is a quite old product, we couldn't debug the code.

While, I find MCF5407 UART driver for your reference.

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,931件の閲覧回数
jbolduc
Contributor I

Hi,

Thanks for the answer. Unfortunately this driver doesn't use the interrupts, but I still managed to find my problem.

The UART interrupt mask register MCF5407_UART0_UIMR and the UART interrupt pending register MCF5407_UART0_UISR share the exact same address. The read operation returns UISR, not UIMR. So we cannot do this :

void EnableTxInt()

{

   unsigned char uimr = CPU_RD(MCF5407_UART0_UIMR); // WRONG !!!
   uimr |= MCF5407_UART_UIMR_TXRDY; // ENABLE TX INTERRUPT

   CPU_WR(MCF5407_UART0_UIMR, uimr);

}

We should do this instead :

unsigned char g_uimr;

// Initialize g_uimr somewhere...

void EnableTxInt()

{

   g_uimr |= MCF5407_UART_UIMR_TXRDY; // ENABLE TX INTERRUPT

   CPU_WR(MCF5407_UART0_UIMR, g_uimr);

}

If it may help someone else.

0 件の賞賛
返信

2,931件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Thanks for the info.

best regards,

Mike

0 件の賞賛
返信