MCF5329RM - cpu clock frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5329RM - cpu clock frequency

1,791 次查看
unixer
Contributor I

Has anyone working with PLL and changing frequency of core ?

 

I am regarding to all kind od experiences and suggestions how to do it?

 

Thanks a lot for any kind of suggestions.

 

Best Regards

 

UL

标签 (1)
0 项奖励
回复
1 回复

1,148 次查看
TomE
Specialist II

The code I'm working on does this. The CPU starts up at 180/60MHz (core peripheral).

 

Very early in our startup/boot we have code that ***

 

 

1 - CHECKS to see what the core is currently running at by looking at the divider,

2 - If it isn't ALREADY at 240/80MHz it then:

3 - Changes to "limp" mode,

4 - Reprograms the clock dividers,

5 - Changes back out of limp mode

6 - Waits for PLL lock (not sure this is needed).

 

There's sample code around that does the above, but don't ask me where.

 

So by now you should be asking "if the CPU runs at 180/60 out of reset, why are you checking to see if it is ALREADY at 240/80"?

 

Because, in spite of what the Reference Manual, CPU Reset does not always reset the PLL. Power-on reset does. The Watchdog reset doesn't. The software-initiated preset probably doesn't either. The external hardware reset probably does.

 

Good luck.

 

0 项奖励
回复