MCF5329EVB - Chip select signals and memory mapping problems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5329EVB - Chip select signals and memory mapping problems

1,762 次查看
mastro
Contributor I
Hi,

I'm using the Coldfire MCF5329 evaluation board and I have to access with the Compact Flash.Which is the initial address that I have to set for read and write to?
The Compact Flash is mapped with the chip select 1 signal, but how can I set it?
How is organized the memory?
Thank in advance!

mastro
标签 (1)
0 项奖励
回复
2 回复数

803 次查看
PaoloRenzo
Contributor V
Depends on how your LCF is organized (how software fits on hardware)
And finally Chips Selects base address configuration is important.
You have to read more about ColdFire or at least entire Chip Select memory chapter

Good luck
0 项奖励
回复

803 次查看
mastro
Contributor I
Hi,

Thanks for the reply Paolo.
I have already read the MCF5329 Reference Manual and the MCF5329 Hardware Specification and
I have set the flex-bus for accessing Compact Flash in this way:

CSAR1 = 0x02000000;
CSCR1 = 0x002A3780; //as MCF5329 Hardware Specification
CSMR1 = 0x01FF0001; // Compact Flash with 32MB of memory

I have try to write from the 0x02000000 address but I can't.
Have I to set something else?
Thank you very much,

mastro
0 项奖励
回复