MCF5329 Compact flash usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5329 Compact flash usage

1,980件の閲覧回数
pmcelwee
Contributor I
I would like to make some kind of bootloader that will read the compact flash and dump a new image down to the nand flash and then (if no card is detected / image found then just take the current image from the nand flash and dump that into ram) take the image on the nand flash load it into the ram and run it.  I can mount the flash in lolo but I can't seem to load the image.bin file from the compact flash into ram and run it.  Is what I am trying to do possible?  I think if I can get this working then I can just put a script into lolo and it should be able to do what I am asking.

ラベル(1)
0 件の賞賛
返信
1 返信

1,265件の閲覧回数
AdamS
Contributor I
Hi,
 
CF is connected (just like on MCF54/7584evb) as memory mapped device. So it can not be accessed as True IDE mode device. In this situation you will not be able to load image.bin file from a CF. You must build your own CF adapter to connect in TIDE mode and using FAT you can access a whole file then.
 
In this current situaltion you could only point to the known fixed memory position to access your image.bin from CF. 
 
B.R.  - Adam 
 
0 件の賞賛
返信