MCF5282EVB flash programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5282EVB flash programming

ソリューションへジャンプ
1,931件の閲覧回数
michaelzhangca
Contributor II

Hi ,

 

I'm using MCF5282evb and using cfflasher to program the flash. I was use PEmicro's parallel BDM debugger , but it dead few days ago. I want to buy the 'USB Multilink Universal' from PEmicro.

 

Anyone knows that if this 'USB Multilink Universal' can be used with cfflasher to program my board?

 

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,769件の閲覧回数
michaelzhangca
Contributor II

I just got the cable, it proves the cable 'Usb multilink Universal' can not work under CFFlasher, I have to use PE's PROGCFZ to program code into flash.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,770件の閲覧回数
michaelzhangca
Contributor II

I just got the cable, it proves the cable 'Usb multilink Universal' can not work under CFFlasher, I have to use PE's PROGCFZ to program code into flash.

0 件の賞賛
返信
1,769件の閲覧回数
Monica
Senior Contributor III

Michael,

thanks much for sharing your experience with Community!

Best regards,

Monica.

0 件の賞賛
返信