MCF5282EVB flash programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5282EVB flash programming

Jump to solution
1,842 Views
michaelzhangca
Contributor II

Hi ,

 

I'm using MCF5282evb and using cfflasher to program the flash. I was use PEmicro's parallel BDM debugger , but it dead few days ago. I want to buy the 'USB Multilink Universal' from PEmicro.

 

Anyone knows that if this 'USB Multilink Universal' can be used with cfflasher to program my board?

 

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
1,680 Views
michaelzhangca
Contributor II

I just got the cable, it proves the cable 'Usb multilink Universal' can not work under CFFlasher, I have to use PE's PROGCFZ to program code into flash.

View solution in original post

0 Kudos
Reply
2 Replies
1,681 Views
michaelzhangca
Contributor II

I just got the cable, it proves the cable 'Usb multilink Universal' can not work under CFFlasher, I have to use PE's PROGCFZ to program code into flash.

0 Kudos
Reply
1,680 Views
Monica
Senior Contributor III

Michael,

thanks much for sharing your experience with Community!

Best regards,

Monica.

0 Kudos
Reply