MCF5282 - Fast Ethernet Controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5282 - Fast Ethernet Controller

2,978件の閲覧回数
venki_02
Contributor I
HI,
               I am a basic level programer in MCF5282. I have been getting confusion about the functionalities of FEC(Fast Ethernet Controller).
              My  confusion is that whether FEC  generate IP address or not. If anybody knows about the
 functionalities of  FEC and IP address generation or any related programs. Please suggest me
in this regard would be helpful for My project requirement.
      
   By                                                                                              
venkat

--
Alban Edit: Message Subject line changed to be descriptive.




Message Edited by Alban on 2007-09-19 11:41 PM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,426件の閲覧回数
Alban
Senior Contributor II
This is a double post identical to HI,                I am a basic level programer in MCF528...

Please note that double posting as well as cross posting is unwelcome on Freescale Community.

This thread is now locked, refer to the 1st subject linked above.
0 件の賞賛
返信

1,426件の閲覧回数
theJoel
Contributor III
Venkat,

The FEC is the Ethernet controller and has no knowledge of addressing at the higher (TCP/IP) layers. The FEC has a physical address that is globally unique, as assigned by the IEEE Registration Authority.

You must program the Ethernet address (the physical address) by writing the PALR and PAUR registers in the FEC.


IP address can be generated automatically, if your application supports DHCP. DHCP is an Application Layer protocol in the TCP/IP suite, the FEC does not interpret these messages.

For more info search "TCP/IP" on wikipedia.org


Regards,
Joel.


--
Alban Edit: Message Subject line changed to be descriptive.



Message Edited by Alban on 2007-09-19 11:41 PM
0 件の賞賛
返信