MCF5282 FEC questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5282 FEC questions

2,813件の閲覧回数
MikeBobowik
Contributor I
Hi,

I am wondering if ECR[ETH_ENABLE] must be set in order to generate MII management frames, and what happens when ECR[ETH_ENABLE] is toggled on/off during communication with an attached PHY device? Also, what happens if the FEC is reset during communication with an attached PHY device?

One last thing, the user manual refers to an "MII_STATUS register" in one spot. What is that exactly?

Thanks,

Mike
ラベル(1)
0 件の賞賛
返信
1 返信

1,373件の閲覧回数
MikeBobowik
Contributor I
Hi again,

After realising I posted this on a Friday, I decided to try and answer my own questions:

As I expected, ECR[ETH_ENABLE] has no effect on the MII.

A reset will completely terminate any communication with an attached PHY device. This means that if I write a routine to read and write PHY registers, it has to be aware of resets so that it doesn't hang waiting for an MII event.

I would appriciate it if someone could confirm this or let me know if I have missed something.

Mike
0 件の賞賛
返信