MCF5235 Pin Config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5235 Pin Config

4,764件の閲覧回数
mcf5235
Contributor I
Hello,
 
Can someone let me know, whats the default pin config for the eTPU on MCF5235 board.It has got 32 channels of which the upper 16 channels are multiplexed with Etherner Controller. So, by default is it totally eTPU? or do we need to program it to use all the 32 channels.
 
Thanks a lot in advance
-Sreekar
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,461件の閲覧回数
Arev
Contributor III
    Hello,
 
The eTPU/EthENB pin configures wich modules are available to the user and selects the muxing of the eTPU Channels (16 - 31) and Ethernet Controller.
  • eTPU/EthENB pin High selects eTPU Channels (16 - 31).
  • eTPU/EthENB pin Low  selects Ethernet Module.

Bye

0 件の賞賛
返信

2,461件の閲覧回数
Ahlan
Contributor III

Hi,

Do you (or anyone else) know of any way that software can read the level of the eTPU/EthENB pin (M4 on the MCF5235) and thereby determine whether Ethernet or 32 channel TPU has been selected at boot time.

Best wishes,

Ahlan

0 件の賞賛
返信

2,461件の閲覧回数
Teddy
Contributor I
Hi,
 
On the evaluation board you have to manage the pin M4 by Switch 7  pin 11. On is Ethernet - OFF is eTPU(16-31).  Zhis is the eTPU/EthEN configuration input pin.
 
Have a nice day
 
Teddy
0 件の賞賛
返信

2,461件の閲覧回数
mcf5235
Contributor I
thts gr8. Thanks a lot for the help.
 
-Sreekar
0 件の賞賛
返信

2,461件の閲覧回数
mcf5235
Contributor I
Hi all,
 
I couldnt use the 32 channels on my board as they are hardcoded as ethernet port...its a CMM5235 but not a 5235EVB.
 
That was the prob.
 
Thanks a lot
 
0 件の賞賛
返信